Industry Online Support
Technical Forum
1/18/2008 8:37 AM | |
Posts: 1776 Rating: (95)
|
Hi, have you seen this FAQ http://support.automation.siemens.com/WW/view/en/11841504 |
2/6/2008 10:50 AM | |
Posts: 9 Rating: (0) |
Hello, i have found the problem it was linked to another one i have. basicaly when i close the winCC project it doesn't close the connections with the data base properly which in turn means when i use project duplicator or save as you can never open the project up again. https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=22091396&caller=view to get round this i have to power the pc off then back on with out starting winCC do the import OS/ duplicate or save as functions. matt |
Last edited by: mattc at: 06.02.2008 10:56 |
|