10/30/2018 6:09 AM | |
Posts: 107 Rating: (0) |
Dear users/specialists/masters could anyone explain what could be the issue with the following: locally in the plc cabinet input signal exists but CPU doesn't see it. (checked several times also reloaded hardware) and this issue related more or less to 0.7 / 1.7 / 2.7 and so on (that consists .7) it is strange because some of the inputs with .7 works fine. before in the commissioning time all was ok tested. for the moment changing that inputs to a free ones. is there any idea ? (power supply for each BU connected) thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/30/2018 11:46:28 AMNew subject after splitting |
|
Follow us on