4/21/2015 1:42 PM | |
Joined: 3/27/2012 Last visit: 9/19/2024 Posts: 179 Rating: (4) |
Hi there, I have some problem in Conversion of I_S and Showing the Recorded Date and Time on Screen (MP277) I have recorded some batches of liquids in a Table (VW192) with the Date/Time of the day, made those batches 14 Records and each Records contain 7 Words (1 word=Mixer No., 3 Words=Date and Time, 1 Word=xx and 2 Words for the amount of liquid used and How much was Required. Copy of Table gone to VW1000 then used Indirect Addressing by &VD2200 Then I used Address of VW3600 in VD2500 to seperate Date and Time from INTEGER Format to becomes as serries of Bytes (I tried even as ASCII (ITA)) but I don't see anything in VW3600 and I don't know where I have gone wrong!!! I attached just the part Record and those functions supposed to make the History page. Function ReadByte7_8 is where Conversions are made. All I need is Date & Time to be saved in a Table then read it from HMI Anybody can help please AttachmentWM-History_Help.zip (280 Downloads) |
Last edited by: Yadi at: 4/21/2015 2:39:12 PMLast edited by: Yadi at: 4/23/2015 9:55:43 AMLast edited by: Yadi at: 4/23/2015 10:06:36 AM |
|
4/22/2015 9:57 PM | |
Posts: 5225 Rating: (1192) |
Could some expert (Marcjan?) or volunteer please help our friend Yadi. |
4/23/2015 4:20 PM | |
Joined: 3/27/2012 Last visit: 9/19/2024 Posts: 179 Rating: (4) |
Hi William, I finally found the problem and now is working OK. There was a couple problem, first I changed Positive Edge detection to a new contact M8.1 and also M11.5 and conversion start to work right, also I had to make the reading from HMI right (Reading right address). I attach the finished one (and again after some minor correction on the history page on Screen) Thank you very much AttachmentWaterMeterProject-03_02_2016.zip (226 Downloads) |
Last edited by: Ahoora at: 4/23/2015 4:21:16 PMLast edited by: Ahoora at: 4/23/2015 4:22:15 PMLast edited by: Ahoora at: 4/23/2015 4:23:15 PMLast edited by: AhooraJafari at: 4/29/2016 10:46:01 AM |
|
This contribution was helpful to2 thankful Users |
Follow us on