5/20/2016 11:50 AM | |
Posts: 5225 Rating: (1192) |
Navnag - Are you listing the Experts that is not Platinum / Diamond? I think our forum friendPiotr.M is not listed yet. |
5/20/2016 1:35 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
Sure, I can do this List of all Experts without Platin/Diamond badge: New Experts: The list of the Platin/Diamond users is right. Best regards |
Last edited by: Min_Moderator at: 5/20/2016 1:36:27 PM |
|
This contribution was helpful to4 thankful Users |
5/26/2016 9:37 AM | |
Joined: 3/14/2008 Last visit: 9/23/2024 Posts: 2096 Rating: (936) |
Maybe just the Gold members/experts? Before you are Gold member, it means that you have already spent a lot of time on the forum. I remember that it took nearly 3-4 months going from Silver (no bars) to Gold (no bars) by spending almost every day on the forum. |
If I could help you, you can use the RATE button. Thank you. |
|
5/26/2016 10:24 AM | |
Joined: 5/20/2015 Last visit: 9/2/2024 Posts: 216 Rating: (3) |
good job navnag and other guys... |
Let's do it... |
|
6/25/2016 10:03 AM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
From what I understand he is already in the list as 1test- he has ( I hope temporarily ) changed his ID to R_I_P as a mark of protest ( 1test -> R_I_P ) |
Last edited by: Navnag at: 6/25/2016 5:02:43 PMThere is no such thing as the last bug in a program |
|
This contribution was helpful to2 thankful Users |
Follow us on