Industry Online Support
Technical Forum
5/4/2011 1:28 AM | |
Posts: 1 Rating: (0) |
Can someone explain what the error message, "inhibit" refers to when I'm trying to run the inverter. |
5/4/2011 3:27 PM | |
Joined: 6/4/2008 Last visit: 5/10/2024 Posts: 1484 Rating: (322)
|
Hi BendyBully, Does the Inhibit message appear on an AOP or are you using Starter? Starter can enable all the relevant bits for you if you take control of the drive with the Control Panel. Either way, please see the attached extract of the Function Diagrams, if you look at parameter: r0054 (Control Word 1), you should see bits 1 through 6 enabled, assuming all is ready to run, if not, investigate which one is disabled. When you give the start command, bit 0 is the last to change. Regards, Graeme AttachmentPages from Function Diagrams - 4150.pdf (106 Downloads) |
Follow us on