Industry Online Support
Technical Forum
10/20/2009 9:06 AM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Darlam , are you trying to modifyin value by CFC chart, using VAT or directly in instance DB? modifying new not connected CFC block or block are you using in your program? there are comunication active with other systems? can you post an example if value are you not able to modify? Reagrds |
10/20/2009 4:28 PM | |
Posts: 4 Rating: (0) |
Hi, I tryed to monitore from a different ES, but with the same project, as I don't know how can I monitore with a different project. The result was the same. I am modifying the inputs in the CFC chart, follow attached two drawings, the situation before and after modifying the input PHH from 100.0 to 100000.0, as you can see in picture 2 the input PH changed alone from 100.0 to -1.3010e-16. There is communication active, ethernet connection to 2 other PLC's (this is a multiproject). Profibus connection to some other PLC's from package equipment in the field, and communication with the WinCC servers, the reason why I started to investigate this problem and found this, is because the communication with WinCC is not working. A complete compilation and full download is out of consideration for the moment because we cannot stop the PLC. Any other suggestions? Regards, AttachmentFB IO problems.zip (44 Downloads) |
Follow us on