2/15/2016 2:21 PM | |
Joined: 12/2/2010 Last visit: 4/11/2024 Posts: 24 Rating: (1) |
Hi, Is it possible to install S7-Graph of Step7 on a PC where SFC is install ? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/16/2016 2:55:35 PMNew subject after splitting |
|
2/16/2016 5:58 AM | |
Posts: 129 Rating: (17) |
You can check the same under 'Compatibility Tool': |
2/16/2016 1:41 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello Idir, No, you cannot use PCS7 with S7-Graph. S7-Graph is released for Step 7 software and you cannot install Step7 software with PCS7 together on one PC. In the tool, you can select PCS7 8.1 SP1 for example and then check if S7-Graph can be added. It it greyed out, which means you cannot select S7-Graph with PCS7 software. SFC is much more advanced and created according with CFC together for PCS7. So Siemens does not bother to use S7-Graph. It's not logic |
If I could help you, you can use the RATE button. Thank you. |
|
3/30/2016 10:00 AM | |
Joined: 12/2/2010 Last visit: 4/11/2024 Posts: 24 Rating: (1) |
Hi, I have install S7-graph 5.3 SP7 on PCS7 V8.1 and it works. S7-Graph only need Step7 5.5 to be installed. |
Follow us on