9/11/2019 9:54 AM | |
Posts: 45 Rating: (0) |
L.S., Yesterday I ran a 'check for updates' and found Upd3 for TIA v15.1 was available. The installed version was TIA v15.1 (without any UpdX). Three Updates where available, if I remember well: Tia Multi Upd3 / Step7 Upd1 / TIA v15.1 Upd3. Since the laptop is full under company-control I had to ask for a temporarily Admin-account. Two of the updates are installed without trouble (as far as I could see). The laptop is installed with Windows 10 Enterprice 2016 LTSB => see attachment Has anyone a clue what the reason for this PopUp could be? regards, AttachmentDriverProblem.zip (26 Downloads) |
9/11/2019 1:14 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello wideko, have you UNICODE characters (for example, Chinese characters) in the installation path. In this case the installation is not possible. The executable file has a digital signature and the server does not receive an answer from the revocation list over the internet. This could be the problem during the installation. Further description and the help is described in the FAQ: Why does the start of the executable file take 30 to 40 seconds when installing STEP 7 (TIA Portal)? With best regards |
Follow us on