Industry Online Support
Technical Forum
10/2/2007 9:22 PM | |
Posts: 1275 Rating: (123)
|
Hi Greg and Amity, There is a patch released specifically for dual core users... you can download it here. There is another patch, patch 3, which can be downloaded here, and corrects bugs which happen with the "GetTag..." function. You should get both of them... Amity, to install WinCC you need to have a communication processor installed, and check the firewall, virus scanner and domain configurations... you should also check compatibility with other Siemens software which may be installed on that computer. Greg, you should check compatibility before upgrading. Remember that when you upgrade WinCC other software which may be installed on that computer may become incompatible with the new version... I've seen installations going wrong, where the only way to get it to work was, like you said, deleting all siemens software completely... but it should have worked after you've done a clean installation of v6.2... Best regards, Danielle |
Last edited by: Danielle at: 02.10.2007 21:30Last edited by: Danielle at: 02.10.2007 21:23 |
|
10/3/2007 2:23 PM | |
Posts: 1275 Rating: (123)
|
Hi Amity, You mentioned Step7 v5.3, right???? Well... Step7 v5.3 isn't compatible with WinCC v6.2 you need Step7 v5.4, with SP1 or SP2. Check the compatibility list here. Best regards, Danielle |