9/23/2016 8:52 AM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
Hi , I have Protool v6.0 + SP2 and now I am trying to install Protool v6.0 + SP3. But installation does not succeed because it keep saying 'You do not have the necessary authorization to install this version. Setup will be terminated.' I followed next procedure . bu after inserting disk I get this message... |
9/23/2016 9:33 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
Which message do you get? Do you have a upgrade version or full? Does the mentioned tipp work? |
~(‾▿‾)~ |
|
9/27/2016 1:15 PM | |
Joined: 11/14/2008 Last visit: 4/24/2024 Posts: 504 Rating: (22) |
Feedback on this issue: I was trying to install the wrong update. My original Protool is Simatic Protool/Pro v6.0 and I was trying to update with Simatic Protool which doesn't work. So after using the good upgrade Simatic Protool/Pro v6.0 + SP3 proof was accepted. Only one other issue was, that it was unable to install SP3 because path of installation file was to deep. Thank to this post I could find the reason back. |
Follow us on