1/5/2011 4:58 PM | |
Joined: 4/8/2008 Last visit: 5/6/2024 Posts: 31 Rating: (2) |
For the network issue; in your virtual machine management area open it's settings and under networking select your network card as a connection. You then must setup your network configuration under the XP machine as you normally would. To get around the remote desktop issue I installed the free version of Real VNC but VNC client/server combination should work. Tiny VNC and Tight VNC are other options. I installed the client and server on each but you need the server on the XP Mode machine and the Client on the Windows 7 machine. |
Glenn |
|
1/6/2011 3:57 PM | |
Posts: 4 Rating: (0) |
Thank you, that has sorted that part and is now fully installed. Patrícia |
1/6/2011 3:59 PM | |
Posts: 4 Rating: (0) |
Thank you!! That worked wonders. It is now installed and working. Patrícia |
2/5/2011 10:56 AM | |
Posts: 54 Rating: (0) |
bit of a bump... can we run Step 7 on our W7 64bit machines yet?? |
3/18/2011 7:17 PM |
|
Posts: 54 Rating: (0) |
Bump again. I have V5.5 for Windows 7 32bit. Any news on 64 bit?? |
Follow us on