(0)| 7/4/2006 1:03 PM | |
|
Joined: 8/31/2005 Last visit: 1/7/2026 Posts: 217 Rating:
|
Hi JW! Have a look in chapter "8.4 Setting the Address Priority (Symbolic/Absolute)" in the "Programming with STEP 7 V5.4" manual. There it is described how to switch names or assignments of symbols in the symbol table. But there is also some mouse clicking... To change the symbol tabel in an automated way you can use the STEP 7 Command Interface. With the STEP 7 Command Interface you can access your STEP 7 project from an Excel macro. With this Excel macro you could export the symbol tabel of your S7 program to an Excel sheet and then programmbeatically change the symbol names and/or assignments. After this you could import the symbols back to the symbol table of your S7 program. For more informations regarding the STEP 7 Command Interface have a look in this thread: Use of Source file. There you'll find the manual and a sample Excel file. |
|
Greetings, Chris |
|
Follow us on