6/18/2014 9:42 PM | |
Joined: 3/5/2014 Last visit: 1/25/2022 Posts: 19 Rating: (0) |
Hello; I want to find a solution about my problem. I have a MP277 panel and I want to take tag log data in my computer. I connected panel and computer same network. I read theProcedure for WinCC(TIA Portal) and Windows 7document. I ping to machine to each other. My computer name is engineercomp. And I ping from panel to computer like "ping engineeringcomp" and I saw communucation everything seems okay. I write log like this "\\engineeringcomp\archive". I ceate a folder in harddisk C and give the name archive. I run the machine but no log data coming from panel to pc. If I am wrong please help me. And the other thing is, how can I see panel screen on my desktop? Thanks for help.
|
6/19/2014 8:21 AM | |
Joined: 4/24/2006 Last visit: 9/18/2024 Posts: 8738 Rating: (1168)
|
Hello bilginer2002, Did you change the "device name" of the panel? When you want to see the screen of your panel on the PC, you will need WinCC Flexible Sm@rtAcces or WinCC flexible Sm@rtService. Best regards, Wizard |
6/19/2014 9:48 AM | |
Joined: 12/16/2012 Last visit: 9/13/2024 Posts: 653 Rating: (130) |
Hello bilginer2002! Are you using TIA Portal? I had to do the same with TIA and a TP277. Unfortunatelly I do not remember why, but it did not work for me so I took a different approach and used a vb script which was running when a tag changed. Here is an example from Online Support for WinCC flex: https://support.automation.siemens.com/WW/llisapi.dll?query=tag+logging+script+windows+ce&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=cseus&objaction=cssearch&searchinprim=&nodeid99=&redir=false I took the "write_data" script and modified it a little bit for my needs (see attachment). It works fine with the TP connected to the PC trough a simple switch. After the TP277 starts up, it asks for the username and pasword of the PC to connect. I created the folder which contains the data log file strait on the C: drive and made it "shared". BR Attila
AttachmentTP277 vbs data log example - TIA portal.pdf (150 Downloads) |
Follow us on