Industry Online Support
Technical Forum
8/21/2010 12:06 PM | |
Posts: 73 Rating: (0) |
Dear all How to integrate WinCC 7.0 in Step 7. So that tags of step7 is directly used in WinCC, without creating tags in WinCC. Please solve my problem. thanks. |
8/21/2010 12:31 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hi Dilip, Here is the Link for the How do you integrate an existing WinCC project into a STEP 7 project? & to take the Tag in WinCC on Compile you have to installed the AS/OS Engineering Option During WinCC Installation, Select the Expert Mode for WinCC V7.0 Also in the Step 7 Side You have to Define the Attribute Which you have to Create the Tag in the WinCC (like S7_m_c) |
Last edited by: Ammy at: 8/21/2010 12:42 PMAmmy |
|
Follow us on