Industry Online Support
Technical Forum
8/30/2005 10:46 AM | |
Posts: 3609 Rating: (29)
|
Yes,I am using the Source-Code,and I have set the parameters about Machine and host correctly. The host can send RPC message to the Machine,and the Machine can to send RPC message back,too.But on the host the VB program can not catch the message! |
8/30/2005 10:47 AM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating: (32)
|
Dear Mr/Ms if you are testing example 1 it's very important to shut down the SINCOM.OCX Testprogram before. While Sincom.OCX is working you can't catch a reply from the machine. If this don't help to solve your problem. Please send the following files to the hotline: Your example 1 with your parameters. For further diagnostic, I need some log-files: \Add_on\SinCOM.log or mcis_rpc.log \Add_on\SinCOMERR.log or mcis_rpcerr.log Start before the following program "\add_on\Scconfig.exe" please Open the strap "Logging" and parameterize as follows: Filesize: 100 Trace level: 4 - After that, delete all log-files - Start MMC - Please after that test the functions with which the problems occurred - copy the logs and send them In addition we need still an excerpt of your Registry Activate following Softkey's on the Windows surface: "Start" => "Run..." write "regedit" => "OK" Then you choose the directory "SINCOM", this file must be exported into a Temp-Directory so that you can send us the so made file. [HKEY_LOCAL_MACHINE\SOFTWARE\Siemens\SINCOM] "Registry" => "Export Registry File..." File name: XXXXXXX "Save" Copy the file "XXXXXX.reg" from the Tmp-list and these send to us. Also we need the \Add_on\scvarset.ini. Best regards Your Technical Support for Automation & Drives SIEMENS AG |
Last edited by: Import-User-2 at: 9/15/2005 2:55 PM |
|