2/26/2019 1:20 PM | |
Posts: 178 Rating: (5) |
How difficult can it be? frustrated! I have a similar problem. I have looked at documentation and at user level settings. I am logged on as an Administrator. I can Stop/Start motors, can change modes etc. However the interlock button remains greyed out and a mystery. OS Perm.Bit ? Feature Bit? Thanks, gbs ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/27/2019 9:45:41 AMNew subject after splitting |
|
2/27/2019 11:10 AM | |
Posts: 64 Rating: (7) |
Hi gbs, Which block is connected to the interlock input on your MotL block? Can you show a screenshot of the CFC chart? |
2/27/2019 11:31 AM | |
Posts: 178 Rating: (5) |
Its a standard library block. I have attached CFC screen shot. Regards, gbs |
2/28/2019 2:20 PM | |
Posts: 178 Rating: (5) |
Any ideas? Have all the experts retired?
gbs |
2/28/2019 2:30 PM | |
Joined: 11/10/2010 Last visit: 4/25/2024 Posts: 165 Rating: (8) |
hello gbs, can you tell us pls if this is the case for all motors or just on motor? and what's your PCS7 version ? |
2/28/2019 3:01 PM | |
Posts: 178 Rating: (5) |
PCS7 v8.1 sp1 Any Motor or Valve block. Thanks |
3/1/2019 12:46 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
I faced this problem before. The issue might relate to server data. If you try to configure a server - client configuration / single OS configuration, it will work. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on