5/19/2013 8:05 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (152) |
I got the same error, look in my posts. /tf/WW/en/Posts/91441#top The problem was in my case using FB with multi-instance, with STAT variables declared as Set in IDB. The solution is to set to retentive, at least to FB's that you are calling. In main FB the Set in IDB can coexist with retentive and non-retentive, as long you don't plan to change parameters on HMI, then there is another mess. TIA =totaly mess up. At time I got this, I spent two days on the battle field, now when I came home I don't have energy to write to Siemens, I was waiting for somebody to step on this minefield.:) |
Last edited by: Marko Bursic at: 5/19/2013 8:17 PM |
|
Follow us on