11/12/2018 3:21 PM | |
Joined: 1/31/2013 Last visit: 3/23/2024 Posts: 32 Rating: (0) |
Hello, In our factory we have a crane and the main hoist has 2 motors each of them 110kW and 2 mm440 inverters 250kW. One on the inverters gives f0001 or f0002 fault then 00010 is shown. I have checked the motors, the cables the resistors and breaking unit 6se7032-7eb87-2da1. All of them are ok, the drivers parameters are same but the fault appears offen. What should I do? Regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/13/2018 10:11:20 AMNew subject after splitting |
|
Follow us on