5/21/2019 7:45 PM | |
Posts: 14 Rating: (0) |
hellow, i have a problem with my io device every 5 -10 minuts when a output from the device is up it gifs these error 16# 02:39CB the lights go out durring this error a few seconds later the error is over en lights go on again what can be the problem of these error? i checket the power suply, i change already the network cable, i look at the module of there is no bad connection in attachment i put my diagnogstics thank you AttachmentDiagnostics.txt (133 Downloads) |
5/21/2019 7:58 PM | |
Posts: 14 Rating: (0) |
hi, i change the power suply from 2.5A to 5 to be sure that this is not the problem, but the 1212dc/dc/dc cpu go not in error, only the io device |
5/21/2019 8:26 PM | |
Posts: 2826 Rating: (684) |
Hello. Building on Hati's notes: What happens if you disconnect all load from the device? BR |