8/11/2021 4:20 PM | |
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666) |
Hello Ahmed.m; Siemens offers (for purchase) a IO-Link library for PCS 7 v9.0, in combination with a IO-Link master CM 4x IO-Link (6ES7137-6BD00-0BA0).from the ET 200SP family. https://mall.industry.siemens.com/mall/en/WW/Catalog/Products/10344274 For more information on this library, you must contact Siemens Codewerk Karlsruhe directly, as shown in the link above; this webpage il give you a bit more information: https://www.codewerk.de/pcs7iol_en/ Information on IO-Link with S7 automation systems is described in the following document: https://support.industry.siemens.com/cs/ww/en/view/65949252/107476560907 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
8/11/2021 4:41 PM | |
Joined: 11/10/2010 Last visit: 4/26/2024 Posts: 165 Rating: (8) |
thank you very much for the feedback, did this CM can be integrated on the ET200sP HA ? i don't have Et200SP on this project :( note : the client want to connect 200 Valve with IO link interface, so will i need 50 Module CM (5=200/4) !!!? thank you |
8/11/2021 5:04 PM | |
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666) |
Hello Ahmed.tn; You are expanding the parameters of your original questio in directions I am not competent to follow. The ET 200SP HA product presentation page does not mention the CM IO-link master module as part of the supported modules, i would presume it is not covered. https://support.industry.siemens.com/cs/ww/en/view/109747953 I would continue to suggest you contact Codewerk Karlsrhe and ask them your questions directly, the Siemens techs would be the best source available to determine how the IO-link master can be deployed in PCS 7. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on