Industry Online Support
Technical Forum
11/28/2012 9:19 PM | |
Joined: 11/26/2008 Last visit: 3/25/2024 Posts: 4 Rating: (1) |
Hello, I want to change a CPU 414-2XG04-0AB0 V4.0 to a CPU 414-3XJ00-0AB0 V1.2 because de first CPU is loaded with almost 256KB code. The second CPU has a bigger work memory. The problem is that in this project an IO-Link 6ES7 138-4GA50-0AB0 with 14 motorstarters is projected. The IO-Link has no trouble with the CPU CPU 414-2XG04-0AB0 but with the CPU 414-3XJ00-0AB0 I can't get it to work. In S7-PCT I see the motorstarters en everything works fine but the CPU doesn't see any I/O. Thank in advance for the answer. AttachmentBasisVerbo.zip (110 Downloads) |
Follow us on