10/22/2019 10:37 AM | |
Joined: 11/17/2016 Last visit: 1/26/2021 Posts: 11 Rating: (1) |
Dear colleagues, is it right that 1.3kHz as sample rate refers to IOT2000 only,and not to the available IO module with analago inputs? And in this context then, what`s about the IO module (6ES7647-0KA01-0AA2) for the IOT2000, what would be the max. sample rate here as I can read faster then 20Hz out from Node-Red. Therefore I do not trust the avalable information from the manual. Also it is not complete here regarding a mentioned "Highspeed Input". What is it by the way at all, this Highspeed Input? I would very appreciate if you could bring light into these things. Thank you very much in advance!!! PS: It would be great to have a possibility to sample at 1.3kHz with an IO module for the IOT2000. Measuring current / voltage from 50/60Hz sources with hall-effect current transducers and doing FFT and THD would be great for a lot of monitoring applications!!! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/23/2019 09:30:57New subject after splitting |
|
Follow us on