9/7/2015 7:11 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello, but don't know what should I do exactly. I called them first in CFC, and I also added redundancy OBs (OB 70, 72, 73)... but the CPU goes to stop when I download the program. Most of the Function blocks in redundancy library have task lists and they are automatically inserted in CFC.The important point is where to insert FB450 and FB451.As starting point, you can check the following application example on AI/AO modules.Always referring to Fault-tolerant system manual is great help. Configuration of Redundant I/O ModulesI hope this helps, hdhosseini |
Follow us on