2/27/2018 9:00 PM | |
Posts: 18 Rating: (1) |
Hi All Is it possible to sort this out? The Default image for IOT2000 devices works fine but up to a point. It has been suggested to use https://github.com/siemens/meta-iot2000 and build an image accordingly but unless you know 100% what you are doing, you might not succeed. Are there any other suggested methods / better build instructions or ready made images available? If we can have an image available to everyone that can be use as is without too much hassle and works out of the box, like any other Linux Distro. |
2/28/2018 3:09 PM | |
Posts: 52 Rating: (2) |
This is the way i found to be the easiest if you do not want to download the "default"- Image. There are several packages needed to build an Image. You can find out on https://www.yoctoproject.org/docs/latest/mega-manual/mega-manual.html which packages you need to install depending on your linux distro. You can download the attached .zip-file "meta-skeletonlayer" and follow these steps: _____________________________________________________________ _____________________________________________________________ I wrote this and created the skeletonlayer to my best knowledge and hope its useful to some. If I made any mistakes feel free to correct them. I started a build process to test the skeletonlayer and it seems to work fine, so I hope it works for you too. Attachmentmeta-skeletonlayer.zip (199 Downloads) |
Last edited by: chris_F at: 2/28/2018 3:15:09 PMLast edited by: chris_F at: 2/28/2018 3:17:25 PMLast edited by: chris_F at: 3/5/2018 2:59:46 PMLast edited by: chris_F at: 3/6/2018 11:34:47 AM |
|
This contribution was helpful to2 thankful Users |
2/28/2018 4:53 PM | |
Posts: 18 Rating: (1) |
Thanks much! Will give it a try and post feedback. |
3/2/2018 12:17 AM | |
Posts: 18 Rating: (1) |
@chris_F Do you perhaps know why I would get this error code?
Log file attached. Thank you in advanced Attachmentlog.do_compile.15301.txt (172 Downloads) |
3/5/2018 8:05 AM | |
Posts: 52 Rating: (2) |
Hi, unfortunately I do not. Did you include a recipe or did you just try to build the Standard Image? Best regards, Chris |
3/5/2018 9:29 AM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating: (43) |
Likely a missing dependency on the host. Double-check the package list that Yocto provides. |
3/5/2018 9:31 AM | |
Posts: 18 Rating: (1) |
Thanks will have a look at that. At least so far your version works better |
Last edited by: Mhew15 at: 3/5/2018 9:32:32 AM |
|
Follow us on