3/19/2019 11:31 AM | |
Posts: 2 Rating: (0) |
Can I use IOT2040 with IO shield to control motorized valves locally and monitor the status online via GPRS as well? |
3/19/2019 1:27 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, with the SIMATIC I/O Shield you have 2 DQs, so you could control two valves. GPRS communication is also possible e.g with a mPCIe card. We have an application example with a 3G modules here. For monitoring you can use node-red, which is the easiest way, because it has an integrated dashboard. But of course you can develop your own webpage. An example can be found here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
4/11/2019 10:48 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, in order to communicate with WinCC you need a driver for the S7 protocol. Here you can find a solution with C/C++. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on