3/31/2020 2:12 PM | |
Joined: 12/15/2018 Last visit: 9/28/2022 Posts: 5 Rating: (0) |
Hi there I recently came across the product announcement for the upcoming IOT2050. I also came across this installation manual. I've been using the IOT2020 and 2040 for a while now and have designed custom casing and a front plate to fit certain shields. I'd love to get started with the IOT2050 as soon as it's released, but I read it'll be until July (Hannover Fair) until it's actually on display. Is there any chance we could get acces to the 3D models of the casing and the device earlier than that? The models provided in this thread for the IOT2020 and 2040 were a huge help to us. Does anything similar exist for the 2050? It'd be awesome if we could get started in CAD even before the actual device is released. Thanks in advance! |
Last edited by: Jen_Moderator at: 04/01/2020 13:27:07Optimized link. |
|
4/1/2020 11:06 AM | |
Joined: 12/15/2018 Last visit: 9/28/2022 Posts: 5 Rating: (0) |
Thanks for the heads up! I had no idea these requests could be created. |
4/1/2020 2:19 PM | |
Joined: 12/15/2018 Last visit: 9/28/2022 Posts: 5 Rating: (0) |
My request was fulfilled, too. Sadly, it contained no 3D models. The accompanied files mentioned "No 3D model available", same for the 2D model. I hope some of the folks working on this device can help me out like they did in this thread. |