5/11/2011 8:07 AM | |
Posts: 799 Rating: (42)
|
HI Jasner,
This is the plc address! You have tu ensure, that you can ping the cpu from the computer. So at first I would recomment you to ensure, that the ip address of the pc is in the same logical network as your PLC. (For this topic you can see this faq. Read the capital: IP-Addressing) When the ping from pc to plc is successful, everything should work fine.(If you don't know the ping command, you will also find description in the faq i postet above) best regards |
5/11/2011 11:22 PM | |
Posts: 10 Rating: (4) |
It is a wincc V7 screenshot David |
3/12/2014 6:05 PM | |
Posts: 3 Rating: (0) |
Dear, AttachmentC:\Documents and Settings\TWAD_CWSS_SEDAPATTI\Desktop\TAG_CONNECTION_PROBLEM1.JPG (481 Downloads) |
This contribution was helpful to1 thankful Users |
6/13/2016 10:20 AM | |
Joined: 1/15/2015 Last visit: 3/22/2022 Posts: 66 Rating: (0) |
I was facing the same problem,But now everything is working well after i changed the logical device address. |
10/30/2017 1:11 PM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8018 Rating: (163) |
New question published by db12@ is split to a separate thread with the subject WinCC can't connect to PLC. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on