9/2/2014 6:38 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating:
|
Which LOGO it should be? |
This contribution was helpful to
1 thankful Users |
9/2/2014 7:03 PM | |
Joined: 2/8/2012 Last visit: 12/22/2014 Posts: 2347 Rating:
|
Such is my suggestion ... |
This contribution was helpful to
1 thankful Users |
9/2/2014 10:23 PM | |
Posts: 5225 Rating:
|
Storage with an update rate.. nice! That was my first thought too.. but then I did a more simplified way. Personally I like yours more than my basic model - especially the update rate. Some notes: 1. Only one storage is needed - use either B003 or B005. 2. SR blocks may give issues when the value is stabilised. I would recommend using TOF instead (as filtered hold). TOF coil driven by the original S and TOR reset by the original R. Thanks for the share! w AttachmentDesign Idea_Detect increasing or decreasing analog input (190B version).jpg (55 Downloads) |
Last edited by: William B. at: 9/2/2014 10:46 PMJPEG attached showing variation on 190B''''s design idea. |
|
This contribution was helpful to
1 thankful Users |
Follow us on