10/14/2012 9:53 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684)
|
Hello m.shoaib khata; Normally, the process image tables are updated at the beginning (inputs)and end (output) of the CPU scan. However, in the S7-400 CPUs and in the more powerful S7-300s (CPUs 317 and 319) you can declare so-called "process image partitions", specified sections of inputs and outputs, that can be updated either; -as part of certain OBs (OB40 to OB47): How do you use or update process image partitions during an interrupt OB? - when called by specific SFCs, called only in the Synchronus Cycle Interrupt OBs (OB61 tp OB64): Automation System S7-400 CPU Specifications: 1.11.3 Isochrone Updating of the Process Image Partition With SFC 126 “SYNC_PI“ you can update a process image partition of the inputs synchronous to the clock. A user program linked to a DP cycle can use this SFC to consistently and synchronously update input data located in a process image partition. SFC 126 can be interrupted and can only be called in OBs 61, 62, 63 and 64. With SFC 127 “SYNC_PO“ you can update a process image partition of the outputs synchronous to the clock. A user program linked to a DP cycle can use this SFC to synchronously update output data located in a process image partition and consistently transmit them to I/O devices. SFC 127 can be interrupted and can only be called in OBs 61, 62, 63 and 64. To be able to update process image partitions synchronous to the clock, all input or output addresses of a slaves must be assigned to the same process image partition. To ensure the consistency in a process image partition during each cycle, the following requirements must be fulfilled for each CPUs: CPU 412: number of slaves + number of bytes / 100 < 10 CPU 414: number of slaves + number of bytes / 50 < 20 CPU 416: number of slaves + number of bytes / 50 < 26 CPU 417: number of slaves + number of bytes / 50 < 20 SFC 126 and 127 are documented in the corresponding online help and in the manual “System and Standard Functions”. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/14/2012 10:09 PM |
|
This contribution was helpful to3 thankful Users |
Follow us on