5/2/2016 7:50 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating: (31) |
hi all, i am going to use S7 1212C first time is it possible to communicate it directly to Wincc SCADA then how? VP |
5/2/2016 7:57 AM | |
Posts: 1529 Rating: (202) |
Which SCADA? Which WinnCC? If it is a current panel/current software (TIA), then no problem. If not, OPC should work. I assume you have PROFINET/Ethernet. |
5/2/2016 8:51 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
If you must use WinCC V7.x then you must use WinCC V7.3 / V7.4 |
There is no such thing as the last bug in a program |
|
This contribution was helpful to3 thankful Users |
5/4/2016 8:21 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating: (31) |
thanks, means if i will use wincc professional v13 then i can get inbuilt driver for CPU 1212C to communicate with it on profinet like in WINCCv7.3 am i right? VP |
Follow us on