11/20/2019 12:24 AM | |
Posts: 16 Rating: (1) |
Hi! Do you know if there is a way to install TIA Portal on a Linux device? If so, what will be the best option to perform this? Thanks! |
11/20/2019 1:33 AM | |
Posts: 1283 Rating: (105) |
TIA PORTAL doesn't support Linux OS |
11/20/2019 7:53 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (77) |
Only using virtual machines. |
This contribution was helpful to1 thankful Users |
11/20/2019 8:20 AM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585)
|
Hi, yes, use Virtual Machine - check also this FAQ: What should you watch out for when installing STEP 7 (TIA Portal) on a virtual machine?Regards, Towome
|
|
|
11/23/2019 3:16 PM | |
Posts: 16 Rating: (1) |
Thank you all for your fast replies. Have a nice day! |
This contribution was helpful to1 thankful Users |
8/6/2021 5:02 PM | |
Posts: 439 Rating: (108) |
Hello, It is possible to do the following with Linux TransferTool, but not program like TIA Portal.
It's more like SIMATIC Automation Tool. Transfer tool - the tool which supports the user when commissioning, servicing and maintaining SIMATIC devices https://support.industry.siemens.com/cs/ww/en/view/109782475 Ordering data Single license Article No.: 6AV6676-6LT00-3YA5 Floating license Article No.: 6AV6676-6LT00-3AG8 Linux Transfertool manual 4.14 Supported OS The following Operating Systems are supported. • CentOS 6 and higher • Ubuntu 16.04 and higher • Debian 9 and higher • openSUSE 15.0 and higher Have a good day! Best regards, HugoD |
Last edited by: HugoD at: 08/06/2021 17:05:19Last edited by: HugoD at: 08/06/2021 17:07:26 |
|
This contribution was helpful to2 thankful Users |
Follow us on