10/4/2016 3:23 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Well, one way is to use: "CUSEQ" to read out the current sequencer and "CUSTEP" to read out the current step. You can then convert this BYTE and WORD to a REAL and use a MonAnL have the sequencer and step archived by setting the .PV_Out with attribute: "shortterm" archiving. Then you can export the TagLogging and read out as .csv or something else. But, one disadvantage I have with the CUSEQ and CUSTEP is that they are created automatically. When you insert a step between steps, the CUSEQ is named to the next free number and they don't align. That's why I always set a stepnumber in SFC directly leading to a MonAnL. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on