6/17/2011 1:32 PM | |
Posts: 378 Rating: (73) |
Dear Experts, I have machine with one HMI MP277 10'' and the hardware had been failed. Thus untill i get part replacement i have replaced by desktop pc with win xp sp2, using Simantic USB PC adapter and wincc runtime. I have done to run .fwx file during computer startup and i make autohide the taskbar. Is it possible to remove all windows environment like taskbar, start menu...etc and display only wincc RT? [schnippschnapp] Many thanks! Splitted from WINCC v7.0 is possible in VISTA HOME PREMIUM?. |
Last edited by: O_Moderator at: 6/20/2011 9:09 AMnew subject after splitting |
|
6/24/2011 12:53 PM | |
Joined: 10/3/2010 Last visit: 5/8/2024 Posts: 1552 Rating: (188) |
make sure you have a way out of this condition first |
B r g d s , |
|
6/28/2011 3:43 PM | |
Posts: 799 Rating: (42)
|
Are you using WinCC (V7 for example)or WinCC flexible (2008 for example)? regards |
6/28/2011 5:57 PM | |
Posts: 378 Rating: (73) |
2008 |
1/28/2020 7:48 AM | |
Joined: 12/16/2019 Last visit: 4/2/2024 Posts: 2 Rating: (0) |
I have the same problem of HMI failure. How did you replaced the HMI with PC? |
Follow us on