8/2/2018 3:03 PM | |
Posts: 1 Rating: (0) |
Hi, my question is that is it possible to use 24 VDC output connection to provide supply for the device, when its not possible to use the network voltage? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/3/2018 6:45:54 AMNew subject after splitting |
|
8/3/2018 7:17 PM | |
Joined: 7/7/2010 Last visit: 9/20/2024 Posts: 15213 Rating: (2417)
|
The 24V provided by the PLC is to provide a voltage for simple switch type devices, not to power up proximity switches, ultrasonic level switches and the like? Limit switch, float switch, pressure switch, things with physical contacts moving, that's what the 24V input supply is intended to source. Anything else, a separate 24V P/S is strongly recommended.
|
science guy |
|
8/13/2018 7:28 PM | |
Posts: 55 Rating: (1) |
I'm sure its just 300-400 mA depending on what model CPU you are using (check the specs). |
Last edited by: kevspark at: 8/13/2018 7:30:20 PM |
|