4/22/2016 8:41 PM | |
Posts: 90 Rating: (0) |
I had to turn ambient lights off.. the numbers are hard to read.. unless you are well aligned with the screen. Something like this.. is much better: |
4/23/2016 2:26 AM | |
Posts: 90 Rating: (0) |
Thanks for the replies .. much appreciated... Look at this: https://www.youtube.com/watch?v=jG_8SRgTWaY
|
Last edited by: The Helping Hand at: 4/25/2016 3:11:18 PMMade the link clickable Last edited by: Lamboom at: 4/27/2016 3:58:30 PM |
|
4/25/2016 3:14 PM | |
Joined: 8/21/2014 Last visit: 5/14/2024 Posts: 954 Rating: (13) |
Click the "Insert link" button in the post editor instead of just pasting the link from the clipboard. A dialog opens then. Paste your link there to make the link clickable.
Best regards The Helping Hand |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
4/25/2016 3:55 PM | |
Joined: 5/28/2008 Last visit: 5/11/2024 Posts: 4506 Rating: (836) |
Dear Lamboom, It's looks good. The better will be if Siemens make it and put online a face plate with this better numeric pad. I am sure that any experienced guy can do it, but also why spend time and effort just to design a keypad?! If Siemens made a better keypad, I will use it, If not I will try to adjust brightness. |
Ayman Elotaify |
|
4/28/2016 1:38 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (192) |
Hello Lamboom, which Runtime do you want to use the NumPad on? Please have a look at this application example:
Here you find a keyboard and a numpad in some different styles in a library and a documentation on how to change it to a style you want. So you can easily increase the size of the test/numbers and the buttons and I/O-fields. (Here is the application example on styles: https://support.industry.siemens.com/cs/ww/en/view/91174767) At the top of the application example you can find an example project where you can have a look at the function. The keyboard/numpad is a faceplate and uses scripts. Therefore you can't use it on a basic panel. It's easiest to use it on a pop-up screen. |
Last edited by: H.J. at: 4/28/2016 1:42:44 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
This contribution was helpful to1 thankful Users |
Follow us on