Industry Online Support
Technical Forum
7/14/2017 9:24 AM | |
Posts: 1 Rating: (0) |
Thank you for the heads up, I have pulled the PSB files from the HMI and keeping them for a back up, I would also like to get a copy of the project as well, do I have to connect Direct to the PLC to get the project ?? is there a way to DL the project from my HMI system, the system is Using a S2-200 PLC with TP177B HMI, I do also have a Siemens PPI Cable on hand. Good instructions on how to get the project would be good,All new to this thank you. ------------------------------------------------------------------------------------------ |
Last edited by: gonebatty at: 7/14/2017 9:27:00 AMLast edited by: gonebatty at: 7/14/2017 9:28:07 AMLast edited by: Jen_Moderator at: 7/14/2017 1:41:02 PMNew subject after splitting |
|
Follow us on