7/28/2021 3:43 PM | |
Joined: 5/16/2018 Last visit: 2/20/2024 Posts: 3 Rating: (0) |
Is there a way to re-run the initial setup from ssh? e.g. change the network interface settings ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/29/2021 08:35:12New subject after splitting |
|
7/29/2021 2:10 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, there is a documentation from Mentor available, it is attached. You can start in chapter 4, the prior ones are not relevant. Chapter 4 is almost the same as chapter 1 in my documentation, in chapter 5 there are some additional topics mentioned. Best regards! Attachmentindustrial_os_iot2050_gs_V2.1.pdf (291 Downloads) |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on