Industry Online Support
Technical Forum
6/1/2011 3:53 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, .MCP is WinCC File Format and .hmi is WinCC Flexible file Format. I am not sure for the coversion of WinCC Project to WinCC Flexible. Dear All, Is there any Conversion available fro WinCC to WinCC Flexible? Splitted from FILE TYPE CONVERSION. |
Last edited by: O_Moderator at: 6/3/2011 10:57 AMnew subject after splitting VANDE MATARAM..... |
|
6/1/2011 6:19 AM | |
Joined: 5/28/2009 Last visit: 5/5/2024 Posts: 127 Rating: (10) |
Dear amit It is not posible to convert wincc to winccflex..... |
Last edited by: MavEric at: 6/1/2011 6:20 AMRegards, |
|
6/1/2011 6:41 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, But you could migrate WinCC to WinCC Flex. http://support.automation.siemens.com/WW/view/en/18796902 ( page 25 - Migrating WinCC projects ) you can see what will receive after migrating.The result is nearly nothing. Better start from the begining and create new project in WinCC Flex. I think this is the right way. Best regards, Hristo Mihalev |
This contribution was helpful to4 thankful Users |
Follow us on