9/22/2010 11:06 AM | |
Joined: 10/7/2005 Last visit: 4/24/2024 Posts: 3004 Rating: (1046) |
Don't mean to dampen your enthusiasms dear Pegaia, but unless STL support will be added too (which is for reasons beyond my imaginationNOT planned as far asI know), we may be out of luck with being able to use existing STLrelated programs in V11 of TIA Portal (which is in general meant to beuseable to program S7-300's & 400's too). It will also be interesting to see what happens if someone decides to program a 300 (or 400) with TIA Portal V11 and someone else will try to use the "classic" Simatic Manager(e.g. Step 7 V 5.5) to make changes to it later on (or vice versa, the way I see it, we may need to prepare ourselves to have and maintain bothsoftware packagesin the not too distantfuture). |
Last edited by: fritz at: 9/22/2010 11:09 AMtypos Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on