Industry Online Support
Technical Forum
4/28/2011 8:13 AM | |
Posts: 691 Rating: (36) |
Dear all Is there any method to create an FC with online Parameter change propert Like I created an FC and used in chart with IOs as constant and downloaded also. Normally While Online mode If I wanted to change the Constant then I have come Offline and change the Value and download it. Is there any Attribute which will be helpful to me for gaining propertties like CHANNEL DRIVERs Splitted from How to create user driver block . |
Last edited by: O_Moderator at: 4/28/2011 8:47 AMnew subject after splitting |
|
4/28/2011 9:07 AM | |
Posts: 183 Rating: (8) |
Hello; If you declare the parameter as input-output instead of input you will be able to go into test mode, see the values (in yellow) and change them. |
6/8/2011 11:00 AM | |
Posts: 73 Rating: (6) |
Dear Shar, Try changing the attributes of required IOs in your FCby assigning it "S7_dynamic = TRUE" and see if it works. Rgds, Krrish!! |
Follow us on