5/13/2020 3:13 AM | |
Posts: 2 Rating: (0) |
Hi all, Is there any way to simply edit a file or add a file on a created wic image? I need to clone a number of SD cards but need to change some settings i.e.: - the IP address in the /etc/network/interfaces file. that will be different for each device/SD card - add a custom node-red module folder Can this be done without messing around with the painful yocto image building? or can you even do it with Yocto?? Any help or ideas would be appreciated! Cheers. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/13/2020 10:30:40New subject after splitting |
|
Follow us on