Industry Online Support
Technical Forum
11/27/2009 7:48 AM | |
Posts: 3609 Rating: (29) |
Import of a technical question of an User senthils wrote: Dear sir, Is this possible to get 0 - 10V analogue output from S7 200/300/400 PLC, When i give digital inputs to the PLC. And vice versa, get the digital outputs, if i give the Analogue input. Any other standard library function available for this query, and give some example program. Thanks in advance. Regards |
11/28/2009 10:06 PM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839)
|
Yes. See the first network of the attached picture. And also you can use unscale function to use physical value.
Yes. See the second network of the attached picture. And also you can use scale function to use physical value. ___________________ Use sclae and unscale from the library: Scale FC: FC105 Unscale FC: FC106 Regards, |
Ayman Elotaify |
|
Follow us on