5/21/2014 12:31 PM | |
Joined: 3/24/2009 Last visit: 6/20/2023 Posts: 535 Rating: (112) |
Dear nandgate, have a look at this link.
Hope this helps! Best regards, yy1 |
This contribution was helpful to2 thankful Users |
5/21/2014 12:31 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
As far as I know , DP master triggers action on DP slave in cyclic manner without any stop (data exchange).With S7 connectionlike what we know as PG operation (or others) via PROFIBUS,this time can be varied in different insatnces.With specific types of DP slaves(or others) , you gurantee a constant interval in each command to outputs.For this case DP master should be class 1 and it is possible in DP bus profile.Read more in the following manual:
http://support.automation.siemens.com/WW/view/en/15218045 |
Last edited by: hdhosseini at: 5/21/2014 12:36 PM |
|
This contribution was helpful to4 thankful Users |
5/21/2014 12:52 PM | |
Posts: 319 Rating: (9) |
The manual was really helpful. Thanks for posting.
|
This contribution was helpful to1 thankful Users |
9/25/2016 2:28 AM | |
Joined: 4/2/2016 Last visit: 6/5/2022 Posts: 6 Rating: (0) |
hi The link you sent require username and password . how should I get to open the link? thanks |
Follow us on