5/9/2021 1:00 PM | |
Joined: 3/5/2018 Last visit: 2/4/2024 Posts: 3 Rating: (0) |
Dear sir, I am also working with antal PDP2CAN i have install Gsd but its showing me that "module configyred but not available" .. its necessary to program some code for this .please reply ------------------------------------------------------------------------------------------ |
Last edited by: usama1233 at: 05/09/2021 13:09:45Last edited by: Jen_Moderator at: 05/19/2021 10:20:53New subject after splitting |
|
5/9/2021 3:40 PM | |
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello usama; Normally there is no required code to connect a Profibus-DP slave to a Profibus-DP master. The only required steps are done in the hardware configuration, where you install the slave'gsd file, then drap a slave icon to the master,s DP network symbol, set the Profibus address on the slave and the data exchage the slave will expect to do with the master. This hardware configuration must then be compiled and down;oaded to the master (the CPU). If you receive a message such as "module configurd but not availavble" it means that the slave's configuration is accepted by the master, but that there is no data exchange with the address or data exchange areas you have set up. There are many threads on the same subject on the forum (it is quite common for beginners to miss a step when setting up a Profibus slave), here is one that shows what items to check out. https://support.industry.siemens.com/tf//ww/en/posts/module-not-available/200035/?page=0&pageSize=10 If everything turns up correct (cable, connector, Profibus address, data exchange areas...) and you still receive ths message, open the CPU's diagnostic buffer to see if any messages are logged there explaining the cause of the error. Use the Save As button i the diagnostic buffer screen to save the logged messages as a .txt file, and attach the file to this thread. That way we can try to fihgure out the problem with you. Hope this helps, Daniel Chartier |
5/19/2021 8:56 AM | |
Joined: 3/5/2018 Last visit: 2/4/2024 Posts: 3 Rating: (0) |
hello Daniel Chartier Sir, Thankyou for replying me.Sir iam using CPU 315 2DP set board rate 500kb on both Master(CPU) and gateway PDP2CAN . Sir i have check all profibus cable connector .all are fine. I have copy GSD file from a machine where same gateway using and its working fine.. But i have observed that the GSD file i upload from that machine and manual of antal PDP2CAN showing some extra Hex parameters. "module configured but not available" where you said . you have to setup for data exchange. so how to do it? i have attached the Diagnose buffer as txt file Thankyou AttachmentDiagnose.txt (160 Downloads) |
Follow us on