5/4/2021 10:21 PM | |
Posts: 2 Rating: (0) |
Hello I think I have a similar issue that also remains unresolved. Maybe we can help each other. This is the status of my expansion card, on Rack0 is on run on Rack 1 on Stop The Sync Modules both show OK and on run. The HW Component are the same. I have try reset on the module. Reset via SIMATIC. I get the CP on RUN but never the CPU. Warn Restart via SIMATIC is usually not possible The message I get is this one Refusal of CONNECT due to different structure of the part AS So far what I have read from other components is that indicated to a memory card.For this CPU this is internal as far as I known. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/05/2021 09:29:46New subject after splitting |
|
Follow us on