8/6/2014 2:20 PM | |
Posts: 5225 Rating: (1185) |
TAGS: S7-1200, firmware 4.0, TIA Portal V13, Web Server, Watch Table, Variable Status, stored Hi there. We are playing around with the newest features of the S7-1200 "loaded" with firmware 4. We are having difficulty to get a function on the Web Server to run. Please see the attached JPEG. We wish to add one of the Watch Tables created in TIA to the Web Server (see image). TIA allows us to do this. The problem comes in when we view the Web Server through a web browser (Firefox / IE / Crome). The user defined Watch Tables are not shown under "Variable Status" as I expect it to be. We have tried the remedy listed in [LINK] - it was not helpful. I have also read through Chapter 11.5.9 Variable Status of the S7-1200's System Manual.. also not helpful. Further searched in the System Manual has shown nothing indicating that adding watch tables to the web server is even possible. Does anyone have any suggestions to get Watch Tables included into the Web Server? Thanks for your consideration. w |
8/7/2014 10:23 PM | |
Posts: 5225 Rating: (1185) |
poke |
8/12/2014 3:39 PM | |
Posts: 5225 Rating: (1185) |
huggy_d1 - good to hear from you. I did not make the support request using the link here. I have asked my friend at Siemens to make the enquiry - hopefully he would also benefit with an answer. I have not yet received an answer.. It would be great if you had the opportunity to play with an S7-1500.. it would however be academical. I have already looked at documentation that shows how it looks like in an S7-1500. I have not yet found any trace of documentation that states how the S7-1200 handles this function. I have a naughty feeling that this web server function is a future development (for the S7-1200) which sneaked its way into the TIA V13 software. I would be very happy to have this function, as we could prepare Watch Tables for technicians (client or ours) to use via the web server to make their work easier. If you do have the opportunity to play with the web server functions on the S7-1500.. please drop me a line. Regards. w |
11/9/2015 1:59 PM | |
Posts: 2 Rating: (0) |
Hi I have the same problem with S7-1200 !! any solution ? If it's not supported by S7-1200 ,why i can add it to my web server!? |
3/2/2016 1:48 PM | |
Posts: 1 Rating: (0) |
I alsohave the same problem with S7-1200 !! any solution ? 1214C FW 4.1 |
Follow us on