7/17/2019 5:14 AM | |
Posts: 6 Rating: (0) |
Hi there, As per title I've been experiencing some massive issues hope someone can help! - long time dweller first time poster. Basically i'm trying to convert a project so I can download it to a S7-1200 PLC (214-1BG40-0xb0) which seems to be available in the later versions of the TIA portal. With this in mind, I did some reading (https://support.industry.siemens.com/tf/WW/en/posts/tip-tia-v14-opening-v10-5-v11-v12-v13-projects/155711?page=0&pageSize=10) and therefore had installed all the apparent prerequisites to make this happen. TIA V12, TIA V13 SP1 and later Win CC updates. However in carrying out the above, I got an error asking me to update Win CC, searched online and found this link:https://support.industry.siemens.com/cs/ww/en/view/58112582 I've attached photos of the errors i've experienced along with the software components installed on the VM i'm using to do this work. Any help would be greatly appreciated as I'm running of ideas of how to solve this. Thanks! |
Last edited by: Jen_Moderator at: 07/17/2019 11:23:34Optimized link. |
|
7/17/2019 5:15 AM | |
Posts: 6 Rating: (0) |
|
7/17/2019 5:15 AM | |
Posts: 6 Rating: (0) |
|
7/17/2019 5:15 AM | |
Posts: 6 Rating: (0) |
|
7/17/2019 6:22 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, you must install WinCC Basic V13 SP1 to update this V12 Project to V13 SP1. Regards Christoph |
7/17/2019 10:26 PM | |
Posts: 6 Rating: (0) |
Thank you Christoph, IT WORKED! |
Follow us on