5/3/2016 4:42 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello I have a few observations : Observation-1 MM420 - Parameter P0210 - Supply Voltage - Can be Set to Zero Volt Does this indicate that Drive can be run without AC input and only DC Supply and will not give Supply under voltage fault Observation-2 In the Post : MM440 SUPPLY CHANGEOVER TO BATTERY BACK UP DURING POWER FAILURE
Observation-3 In the Post : Is it possible to supply a Micromaster with DC batteries through the DC link?
These observations seem to confirm that it is possible to operate MM420 with ONLY DC supply. Maybe the Experts can provide their openion . Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
5/4/2016 9:54 AM | |
Posts: 198 Rating: (36) |
thanks navnag |
Follow us on