4/1/2019 11:09 AM | |
Joined: 5/1/2015 Last visit: 5/10/2024 Posts: 102 Rating: (0) |
Hello again, I have some errors. Maybe someone can help me. 1.I have an FB for Axis and for 2 from 5 it is ok. I mean if i push "job positive" it is working in right direction. But from 3/5 Z-Axis is not ok. If I push "Job negative" is moving down. The same for "Job positiv". It can be something wrong in TO?Then if I push a little bit more then it come this error : "Technology alarm 542 Alarm reaction: Remove enable Restart: Not required Alarm text Solution Clamping monitoring error: Axis leaving clamping tolerance window. The axis has executed a motion greater than the permissible tolerance at the fixed stop. Check whether the fixed stop has broken away." -I've check everything and it is ok. 2. When I compare p98 with p97 in parameterlist there is a difference. I've made like in Operating Manual : p9 active and then it says that should p98 with p97 equal. It doesn't happen.Why? 3.I'm sure I will have some problem at Safety activating. I will try this one later. Can anybody help me? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/1/2019 12:23:54 PMNew subject after splitting |
|
4/2/2019 8:44 AM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8018 Rating: (163) |
Closed cause questions posted twice. The several threads with the subjects "Job negative" is moving down, Compare p98 with p97 in parameterlist and there is a difference?, How to activate the safety correctly? is published within the conference SINAMICS.
Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on