3/16/2017 2:45 PM | |
Posts: 107 Rating: (0) |
Hi everyone, I have question not related to siemens but may be some of you had deal with it before. I've blown my mind with Jumo dTRON 308 trying to activate SP2, SP1 is active always but even switching to SP2 is not possible, type is 703043/181-140-23/000 is standart with 2 relay output. My idea is For example: SP1 = 50 and SP2 = 100 when SP1 reached I shuld have relay one is ON then when SP2 reached relay 2 is ON Now I have like this <SP1 relay 1 ON then >SP1 relay 2 ON...... nothing more it's very strange (spent on this 3h) If someone knows (manual useless) later want to try with software may be will help. Thank you all. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/17/2017 2:05:40 PMNew subject after splitting |
|
3/24/2017 7:14 AM | |
Posts: 107 Rating: (0) |
Solved with dTron software. thanks. |
Follow us on